Setting up a sequence on the QD104 series

Issue

How to setup a sequence on the QD104 series

Product Line

Other, Pelco Cameras

Environment

QD104 series

Cause

Program Sequences

Resolution

 

 

Sequencing

The Default sequence is all cameras 1,2,3,4, Quad

 Programming

To program cameras to a sequence on the call monitor:

  1. Hold in the sequence button on the left side of the front panel until the LED begins blinking.
  2. Select the cameras to include in the sequence by pressing the desired camera buttons ( 1,2,3,4, quad)
  3. Press the sequence button.
  4. Select one of the four dwell times by pressing a camera button.
  • Camera 1 = 2 seconds ( default)
  • Camera 2 = 4 seconds
  • Camera 3 = 8 seconds
  • Camera 4 = 16 seconds

        5. Press the sequence button. The sequence begins.

Operation

To start and stop the sequence

  1. Press the sequence button on the left side of the front panel to start the sequence.
  2. Press the sequence button again( or any camera button) to stop the sequence.