Can I convert an NSM5200 network-storage manager to a fibre-channel model?

Issue

The NSM5200 comes in two base models -- the NSM5200 and the NSM5200F.

Product Line

Pelco Video Management

Environment

NSM5200 network-storage manager, all versions

Cause

The NSM5200F is an NSM5200 with an NSM5200-FC card installed. No other hardware differences exist.

Resolution

This is a direct fiber connection for storage. Yes. Simply install the NSM5200-FC fibre-channel expansion card. For instructions covering how to install the fibre-channel card, please click here.