Is serial tunneling (to Network 8000 controllers) possible through an Automation Server?

Issue

Is serial tunneling, using XPSI to Network 8000 controllers, possible through an Automation Server?

Product Line

SmartStruxure Solution

Environment

Automation Servers (all revisions)

Cause

Remote connectivity to Network 8000 controllers in a building is a desired feature

Resolution

There is no serial tunneling with XPSI available from Schneider-Electric.

The Communities website may offer an option:  http://buildingscommunity.schneider-electric.com/message/19504#19504