Upgrading Reports Server to 1.5 and receiving notification that SQL2008 R2 SP2 is not installed

Issue

Upgrading Reports Server to 1.5 and receiving notification that SQL2008 R2 SP2 is not installed

Product Line

SmartStruxure Solution

Environment

Reports Server

Cause

Web Reports 1.5 requires that the express version of SQL2008R2 be at SP2, prior to 1.5, the site could use SQL 2008 R2 SP1 or RTM.

Resolution

  1. Download the update for SQL which installs 2008 R2 SP2 at this link: http://www.microsoft.com/en-us/download/details.aspx?id=30437 Use the File ending in -x64-ENU
  2. Run the executable file after it downloads
  3. Install StruxureWare WebReports 1.5 using the Upgrade Database option