What are the requirements for the DX8100HDDI to interface with the DX8100 Series HVR?

Issue

The DX8100HDDI is the only external storage system supported for the DX8100 HVR.

Product Line

Pelco Video Management

Environment

  • DX8100HDDI
  • DX8100 series

Cause

Sales Support

Resolution

The DX8100-ISCI SCSI card is required to interface the DX8100HDDI to the DX8100 series HVR.

However, due to hardware limitations the DX8100 SCSI card only works with the DX8108 and DX8116.

NOTE: The DX8100HDDI does not work with the DX8124 and DX8132 because these units do not have a viable slot available for the SCSI card.