Will the FD-FK flush kit work with the FD2 or FD5 camera?

Issue

Flush mount compatibility for the FD2 and FD5 series camera

Product Line

Pelco Cameras

Environment

  • FD2
  • FD-FK
  • FD5

Cause

Flush mount compatibility

Resolution

The FD-FK flush kit is compatible with both FD2 and FD5 Series indoor and outdoor installations

The FD-FK flush kit, FD-WM wall mount, and FD-AP 4S electrical box adapter plate are compatible with both FD2 and FD5 Series indoor and outdoor installations

Note: FD-WM is recommended for indoor only with both FD2 and FD5 installations.

 

 

 

 

 

Related topics:

   4S Electrical adapter plate for FD2 or FD5