Relay Output Installation on DX8100 Series Hybrid Video Recorder

Issue

A Relay is not getting trigger on the DX8100.

Product Line

Pelco Video Management

Environment

DX8100 Series

Cause

Relay is not getting trigger due to incorrect wiring.

Resolution

To wire a relay output.

  1. Insert the blue terminal block into the relay sockets on the back panel of the recorder.
  2. Connect one wire from the device to one of the relay output terminals 1 through 16.

    Relay outputs do not have to correspond numerically to alarm inputs. All sensor input and relay output actions can be linked through programming.
     
  3. Connect a second wire from the relay device to a GND terminal.

            

Note: The DX8100 has either 8 or 16 relay outputs depending on your system's configuration. Each output is programmed to function as either a Normally open or Normally closed circuit.  A signal from a relay output  will operate the device connected to the output. The maximum relay power rating is 120VAC, 0.5A; 24 VDC, 1A.


Related Article:  Linking Relay Output to Motion Event