Operating System + SQL Server only allowed to be English versions

Issue

Does the Operating System + the SQL Server needed to install the reporting package for the SmartStruxure platform only allowed to be English versions

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site with Reports Server

Cause

Help.SBO states:
Microsoft provides a number of versions of SQL Server. In order to install and run WebReports with Building Operation, you need to download and install SQL Server 2012 Standard, 64-bit (or Express with Advanced Edition, 64-bit). Do not install any other version of SQL Server. You can download the executable file for 64-bit operating systems:

SQLEXPRADV_x64_ENU.exe.

Does the Operating System + the SQL Server needed to install the reporting package for the SmartStruxure platform only allowed to be English versions or we could go for an Spanish/German/etc. version for both of them?

Resolution

WebReports is not supported on non-English platforms.