Do you sell parts of the FEXTPS power supply that will work with the new 10-bit fiber modules?

Issue

Do you sell part of the FEXTPS power supply that will work with the Comnet fiber?

Product Line

Pelco Transmission & Power

Environment

FEXTPS

Cause

Customer has lost a part that shipped with the FEXTPS.

Resolution

Unfortunately, in this instance, there are no extra parts for the FEXTPS units and there will be a need to replace the complete FEXTPS unit in total if parts were missing or lost out of the original contents.