ilon600 and SBO

Issue

ilon600 and SBO

Product Line

SmartStruxure Solution

Environment

SmartStruxure Enterprise Server

Echelon iLon600

Cause

Whant to use ilon600 in SBO

Resolution

There are no support for Ilon 600. Stuxurware only supports Loytec network interfaces. See datasheets for exact models.
So if you are engineering a new system you should get Loytec products.

However the Loytec NIC has support for Ilon600 so you should be able to add a NIC852 and one L-IP (to use as a config server) and use the ilon600 as router. But as fas as I know this have not been tested but should work.

But the only supported interfaces are the ones listed in the datasheet.