Can I export a map from Endura Mapping with the icons and text included in a single file?

Issue

The customer wishes to create an image or PDF of the map shown in Endura mapping to be viewed outside of the Endura system.

Product Line

Pelco Video Management

Environment

Endura Mapping, all versions

Cause

Endura Mapping does not have an export feature that combines the text and image in one file.

Resolution

None at this time. You can only export a backup to re-import back into Endura Mapping. You can also back up the mapping background image. But the icons and the map-data file are exported as two separate files.