Reference to the EH3512-2 enclosure fan?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

  • What is the fan part number for EH3512-2?
  • Can I purchase the EH3512-2 enclosure's fan separately from the enclosure itself?

Product Line

Other, Pelco Cameras

Environment

EH3512-2

Cause

Fan failure on EH3512-2.

Resolution

Here is the fan part number for the EH3512-2 enclosure's fan: FN02-4305-4300.