Lua Program for DIM Digital Input modules

Issue

Require a Lua script for using DIM modules

Product Line

SmartStruxure Lite

Environment

SmartStruxure Lite

Cause

Using a Digital Input Module and Lua script is required to view the Inputs.

Resolution

For Sontay's DIM4 module download the script here.

For Sontay's DIM6 module download the script here.

For AXIO's DIM module download the script here.

For a generic DIM module download the script here. The voltage received at the AI may need tuning.

Copy and paste the text into a Lua program and create the Binary Values (BV).