Issue
Questions on whether other fonts be added to EpiDesigner EpiBuilder
Product Line
Andover Continuum
Environment
EpiBuilder
EpiDesigner
Windows XP
Windows 7
Windows Server 2003
Windows Server 2008
Cause
The method to add fonts to EpiDesigner is needed to use alternate fonts
Resolution
- Download or install the font that is needed to a folder on Windows
-
Unzip if necessary and then drag and drop the font file(s) into the windows fonts folder and they should automatically install.
Here are some Windows instructions for installing manually. http://windows.microsoft.com/en-us/windows-vista/install-or-uninstall-fonts - After installing the fonts you can open a layout in EpiDesigner and select the newly added font.