How to turn on Auto Focus on Spectra camera using a KBD300A keyboard

Issue

Enabling Auto focus

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • KBD300A keyboard
  • Spectra III
  • Spectra IV

Cause

Unable to auto focus during zoom in or zoom out

Resolution

  1. Using a KBD300A keyboard, enter 95 then push and hold Preset for a few seconds, a small menu appears
  2. scroll/toggle down to SET, "S" should be flashing, and  then toggle joystick to the right
  3. Camera menu appears, arrow should be on Camera, push "Iris Open" key to enter camera menu
  4. toggle/scroll down to Auto Focus and push the Iris Open key, this moves the arrow to the right enabling the ability to turn on or off the Auto Focus feature
  5. Toggle the joystick up or down to change the state from off to on (to turn auto focus on), or vice versa
  6. Push the Iris Open button to enter the function (the arrow moves back to in front of Auto Focus
  7. Toggle/scroll down to Exit