What is the replacement unit for the VS5004 and VS5008?

Issue

What is the replacement unit for the VS5004 and VS5008?

Product Line

Pelco Cameras, Pelco Monitors, Pelco Matrix

Environment

  • VS5004
  • VS5008
  • VS5104
  • VS5108

Cause

Customer request for a replacement for the VS5004 or VS5008.

Resolution

The replacement models for the VS5004 and VS5008 will be the VS5104 and VS5108. 

Note: These replacements do not have the alarm inputs that the previous versions were capable of.

More information can be found on the VS5104/VS5108 on the Specification Sheet linked Here.