Change the IP address of a server after having added it to a PCS project

Issue

How can I change the IP address of a server (ES or AS) after having added it to my PCS project

Product Line

SmartStruxure Solution

Environment

Project Configuration Server

Cause

You can't change the IP address of a server in the properties for that server

Resolution

1. Click on the project

2. Click on "Servers"

3. Click "Properties"

4. Click on the server which IP address you wish to change

5. Change the IP address and click save