What do the LEDs mean on a CM9765/70/80 Matrix Bays?

Issue

What do the LEDs colors represent on CM97XX-VCC and CM97XX-VMC cards?

Product Line

Pelco Matrix

Environment

Versions 9.03 and above.

  • CM9765-MXB
  • CM9770-MXB
  • CM9780-MXB

Cause

LEDs blinking on CM97XX Matrix Bay. What does it indicate?

Resolution

The LEDs is a basic check of the system operating properly. Various LEDs will blink during the initialization process as the software verifies communication and version level information.

  • Table K displays the settings on a CM9765-VMC card.
  • Figure 40, Table I and Table J are settings for CM9770/80 MXBs.