Does the SE8000 product have a heat pump application?

Issue

Does the SE8000 product have a heat pump application?  There are only fan coil control applications available.

Product Line

TAC I/A Series

Environment

SE8000 controllers

Cause

End customer requests

Resolution

Heat pump applications for the SE8x00 product are scheduled for availability in the 4th quarter of 2014.