Smart Sensor will not display room temperature using a simple program on B3 controllers


Configuring a Smart Sensor in a B3 controller in StruxureWare Building Operation using a simple script program to display temperature. The temperature does not display in the Smart Sensor LCD.

Product Line

SmartStruxure Solution


Automation Server with B3 controllers


SmartStruxure 1.4 attaches a _AV, _BI, etc. to the BACnet name


  1. Remove the _AV, _BI, etc. from the LCDDisplay BACnet name
  2. Download the controller again
  3. The display functions as suggested