NIC-USB cycling between online and offline when setup as a LTA.

Issue

Looking at the properties of the NIC-USB in workstation the status changes from Online to offline over a 5-10 second cycle

Product Line

SmartStruxure Solution

Environment

SmartStruxure 1.5

Cause

The NIC-USB is set up as an application

Resolution

In the Loytec LConfig software select the Advanced button and make sure that "Run as Service.." is selected.