What sensor element is used in STR300?

Issue

What type of sensor element is used in the STR300?

Product Line

TAC Vista, Field Devices, SmartStruxure Solution

Environment

STR300

Cause

The HVAC European+Sensors+Catalogue.pdf on the Extranet, as well as the datasheet for the STR300 Series says that the sensor element is PT100 Class B.

Resolution

The actual sensor element for the STR300 that are made today is NTC Thermistor 10 kOhm.

The output from the STR300 is 4-20 mA.

 

The documentation will be updated shortly.