Create a RAID on DX9100.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Create a RAID on DX9100.

Product Line

Pelco Video Management

Environment

DX9100 series

Cause

BIOS level RAID setup on a DX9100.

Resolution

BIOS level RAID setup.

     

  1. Boot up the Recorder and press [Ctrl] [H] when prompted to run BIOS RAID setup
    utility.
     

     
  2. Use the Up/Down arrow on the keyboard to scroll to Create Array and press [Enter].
     
  3. Select Array Mode and press [Enter].
     
  4. Select RAID 0 (Striping) for performance and press [Enter].
     
  5. Scroll down to Select Disk Drives and press [Enter].
     
  6. Press [Enter] on each drive to add them to the array.
     
  7. Scroll to Block Size and press [Enter].
     
  8. Select 128K and press [Enter].
     
  9. Scroll to Start Creation Process and press [Enter]. A message will appear warning
    that all data on the selected disks will be deleted. Press [Y] to confirm.
     
  10. The menu will default back to Create Array. Press [Esc].
     
  11. Press [Y] the Recorder will reboot.