How to run the DX9000 client configuration utility.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

The DX9000 server name is not in the DX9000 client configuration utility.

Product Line

Pelco Video Management

Environment

DX9100 view station

Cause

  • DX9000 server name was removed from the DX9000 client configuration utility.
  • DX9000 server database was rebuilt.

Resolution

Run Client Configuration utility:

Note: Make sure the DX9000 Viewstation application is closed before opening the Client Configuration Utility.

  1. Go to Start > Programs > DX9000 Viewstation > Client Configuration Utility. The following dialog box appears.
     

     
  2. Enter your user name and password. (default user and password "admin")
     
  3. Click Login. The following dialog box appears.


     
  4. Select “Build a list of local servers
    1. Standard naming: Select this option if all recorders have the same name and the only difference is the numbers. Example, pelco1, pelco2, pelco3.
    2. Custom naming: If your recorders have different names, enter the names and then click Add.
       
  5. Click Configure. 
     
  6. Select “Export to server.”
     
  7. Select the name of the first recorder from the drop-down box.
     
  8. Click Configure.
     
  9. Click Close.