Adjusting the Camera Position for FD5 Series

Issue

Adjusting the Camera Position for FD5 Series

Product Line

Pelco Cameras

Environment

FD5 Series

Cause

Field of view

Resolution

Adjusting the Camera Position:

The dome camera has three axes for positioning the camera. While monitoring the picture on the monitor, adjust the camera position as follows:

  • Pan adjustment:  Rotate 3D assembly in the base.  Do not turn assembly more than 360 degree as this may cause the internal cables to twist and disconnect or break.
  • Tilt Adjustment:  After loosening the screw on the bracket, position the camera as desired, and then tighten the screw back to the bracket.
  • Horizontal Rotation:  For wall mount and tilted ceilings, rotate the lens base (maximum 360 degree) until you are satisfied with the field of view.


Adjusting the Lens (if equipped with vari-focal lens)
 

  1. Loosen the zoom lever (#4) counter-clockwise a little, and then rotate the zoom lever and determine the image view.
  2. Loosen the focus lever (#5) counter-clockwise a little, and then adjust the focus for optimum picture sharpness.
  3. Re-tighten the zoom lever and focus lever after adjustment.

Note:  It is important that you lock the zoom and focus levers after making adjustments.  This will prevent the positions from moving (for example, from temperature changes or vibrations)



 

 

Click HERE for FD5 Series Installation Manuals