Installing Webclient over the top of Cyberstation


At times a webclient install is needed but a Cyberstation installation was done

Product Line

Andover Continuum



Windows XP

Windows 7

Windows Server 2003

Windows Server 2008


If only Cyberstation was installed, but webclient is needed will installing webclient over the top work


The recommended installation of webclient when Cyberstation has been installed first is as follows:

Uninstall of Cyberstation, reboot and then a install webclient. Trying to install over the top will not install the needed web components.

You should run the C:\Windows\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i command after the install to re-register .net framework with IIS.