Changing the comm port for a Menta application RS232 direct connection with no Vista installed

Issue

On a SmartStruxure workstation PC how can the Menta communication port be changed.

Product Line

SmartStruxure Solution

Environment

SmartStruxure 1.5

Cause

The Menta setup application is not added in the start menu.

This exe is located in the StruxureWare install files and can be run to change the communication port for a direct RS232 connection

This file is located in the following directories

64bit systems

C:\Program Files (X86)\Schneider Electric StruxureWare\Buildings Operation 1.5\Workstation\Menta Setup.exe

32 bit system

C:\Program Files\Schneider Electric StruxureWare\Buildings Operation 1.5\Workstation\Menta Setup.exe

Resolution

Run the Menta Setup.exe and add the communication port that Menta will use.

For the first time the other settings must be entered as detailed in this image.