What is the replacement unit for the FT82041 or FR82041 Unmanaged Ethernet Switch?

Issue

What is the replacement unit for the FT82041 or FR82041 Unmanaged Ethernet Switch?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • FT82041 / FR82041 Series Unmanaged Ethernet Switch
  • FUMS-F Series Unmanaged Ethernet Switch

Cause

Customer request for replacement unit for FT82041/FR82041.

Resolution

The replacement for the FT82041/FR82041 Series Unmanaged Ethernet Switches would be the FUMS-F Series Unmanaged Ethernet Switch. These units have different models depending on need or system design. Some models will require a separate FSFP module in order to connect fiber between the two units.

More information on the specifics of the FUMS-F Series can be found on its specification sheet located Here.