Vista - Xenta server offline

Issue

Xenta Server is offline in Vista and can not be reached via web interface.

Product Line

TAC Vista

Environment

  • Vista 5.1.9
  • Windows 7

Cause

The PC has proxies configured.

Resolution

  1. Open Internet Explorer
  2. Go to Tools > Internet options > Connections > LAN settings
  3. Disable "use a proxy server"

Related Article: Lessons Learned Article #12569