How to reboot and reset the Sarix TI Thermal IP Positioning System/fixed camera

Issue

How to reboot and reset the Sarix TI Thermal IP Positioning System camera

Product Line

Pelco Cameras

Environment

Sarix TI Thermal IP Positioning System/PTZ

Sarix TI fixed

Cause

Reboots the camera or Restore the camera's factory default settings.

Resolution

  • Using a small tool, such as a paper clip, press and release the Reset button once to reboot the camera.
  • Press and hold the Reset button for 10 seconds to restore the camera to the factory default settings.
  • Default IP address:  192.168.0.20