Newly-Added IP PTZ Cameras are Treated as Fixed Cameras in Endura


A newly-added IP PTZ camera is added to an Endura system. However, the WS5000 program does not seem to recognize it as a PTZ camera. When hovering over the video, a standard mouse pointer is displayed instead of crosshairs.

Product Line

Pelco Video Management


WS5200 Advanced System Management Software, all versions
VCD5202 video console display, all versions
ExSite IP Camera, all versions
Spectra IV IP H.264, all versions
Esprit IP camera, all versions


The Endura system does not recognize that the camera is a PTZ model.


  1. Open the WS5200 program.
  2. Right-click on the camera with the issue and choose Modify settings.
  3. Verify that the camera type is set to either Dome or Pan and Tilt and that the protocol is Pelco D. By default, Endura will not allow you to change these values.
  4. Click OK
  5. Drag the camera back into the video pane.
  6. Note that the standard mouse pointer has changed to a crosshair pointer.