What are the Fan Specificationssize of the fan on a LB1000 Lockbox

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

Fan size and part number used in the LB1000.

Product Line

Pelco Transmission & Power

Environment

  • LB1000

Cause

  • Sales Support

Resolution

Here is the size of LB1000 Fan: 120X120X38MM.

Here is the Fan part numbers: FN02-1402-1300.