How many relay packs could be connected simultaneously to one SE7300 or SE8300?

Issue

How many SC2300 could be connected to one SE7300 or 8300?

Product Line

SmartStruxure Lite

Environment

SC3000 SE7300 SE8300

Cause

Inputs from the relay packs could not be connected in parallel.

Resolution

It is not possible to connect inputs in parallel, therefore you could only connect one relay pack to one device.