Which 2 wires do I use for 24 VAC or 12 VDC for the IS50 camera?

Issue

Which 2 wires do I use for 24 VAC or 12 VDC for the IS50 camera?

Product Line

Pelco Cameras

Environment

  • IS50 series
  • IS20 series

Cause

Installation for 24 VAC for the IS50?

Resolution

Click on picture below to enlarge