Pelco D control over Ganz PTZ cameras.


How do I set up Presets from a KBD300A to the Ganz cameras.

Product Line

Pelco Cameras, Pelco Matrix


  • CM6700 and CM6800 set to "D".
  • Ganz PTZ camera models.


Minimal reference available for the Pelco to Ganz integration.


For great reference - Ganz reference material. This is depicting the exact way our cameras can be programmed for either Presets or Patterns from a KBD300A. This just so happens  to depict a CM6700 in the line, but, with it being Pelco "D" or "P", and their cameras accepting the same Preset numbers, the functions remain the same across systems for programming Presets and Patterns in the Ganz cameras.