dwg import to Graphic Editor fails

Issue

Importing of AutoCAD .dwg files fails to import into StruxureWare Building Operation Grahics Editor

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site

Cause

Importing of AutoCAD .dwg files fails to import into StruxureWare Building Operation Grahics Editor

Resolution

It is the third party library Leadtools that fails to convert the file. The files in question are constructed with version post 2010 but our Leadtools library is from 2006. To fix this issue the Leadtools library needs to be updated. This will be fixed in a future release. The dwg drawings will need to be saved in an earlier release for compatibility with Graphics Editor.