How to configure PTZ control using the DX Series Client connected to a DX DVR/HVR.

Issue

How to configure PTZ control using the DX Series Client connected to a DX DVR/HVR.

Product Line

Pelco Video Management

Environment

  • DX Series Client
  • DX4700/DX4800(HD)

Cause

New install of coaxitron camera and need to setup PTZ control.

Resolution

Using the DX Series Client connect and login to DX HVR.

  1. Go to the Setup (gear icon)
  2. Go to Display
  3. Select the Channel number
  4. Select PTZ settings - Coaxitron = Port - Coaxitron, Protocol - Pelco C, address and baud rate can remain at default.
  5. Exit Setup by clicking the live icon, when prompted click Save to apply settings