Analog output tour displays only on half of the screen.

Issue

When configuring a camera tour on the ENC5416 Output 1 it displays al 8 cameras but only uses half of the screen.

Product Line

Pelco Video Management

Environment

  • DSSRV
  • ENC5416
  • ENC5400 Host Card

Cause

The ENC5400 Host card is installed in the incorrect PCI-e 4X slot

Resolution

Move the ENC5400 Host card into the PCI-e 16X slot