How do I Connect the Sarix Professional IMP series Indoor Pendant to the WMVE-SW mount.

Issue

Unable to wall mount the Sarix Professional IMP series Indoor pendant camera.

Product Line

Pelco Cameras

Environment

  • Sarix professional Indoor Pendants
  • IMP519-1P
  • IMP319-1P
  • IMP219-1P
  • IMP1110-1P
  • IMPS110-1P
  • IMPBB-P
  • IMPBB-EP
  • WMVE-SW
  • MF00-A360-156A

Cause

Sales and Support

The Indoor pendant doesn't have any mounting threads.

Resolution

ALL Sarix professional IMP series Indoor pendants use the .75" to 1.5" NPT adapter supplied with the WMVE-SW mount. The WMVE-SW  MUST be purchased with the IMPBB-P for mounting.

IMPBB-P - IMP series INDOOR Pendant adaptor