Is it possible to have audible alarms in WebStation?


How doe the functionality differ between Webstation and Workstation?

Product Line

SmartStruxure Solution


StruxureWare Building Operation 1.5 WebStation


Alarms can be viewed in WebStation but they do not have audible alarms sound. 


Audible alarm sound feature is not available in the WebStation. Refer to the following for a summary of the features available:

StruxureWare Building Operation 1.5 User Interface Summary

StruxureWare Building Operation 1.6.1 User Interface Summary