Wink cycle attached to a circuit that is attached to more than one zone on which zone will it work?

Issue

If a wink is attached to a circuit that is attached to more than one zone on which zone will it work?

Product Line

TAC I/NET

Environment

I/NET site

Cause

Wink cycle attached to a circuit that is attached to more than one zone on which zone will it work?

Resolution

If you have a circuit attached to more than one zone with a wink cycle on it, the circuit will wink on the zone that turns off last. If you have a circuit attached to two zones and both zones turn off the lights at five, then the wink cycle will start at five.

 

If you have a circuit attached to two zones and one zone shuts off at five while the other zone shuts off at six, then the wink cycle will begin at six. One more example, is if the zone is set to two different zones and the zones are at different times. One is from seven to five and the other zone is on from eight to eleven, then the wink cycle will work at five then at eleven.