Will the WCS1-4 support 240 VAC input.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

The WCS1-4 is a single channel power supply designed for indoor or outdoor applications.

Product Line

Pelco Transmission & Power

Environment

  • WCS1-4 Series Power Supply

Cause

  • Sales Support

Resolution

WARNING: The WCS1-4 does not have an on/off switch. Turn off power at the circuit breaker before wiring the power supply.

The WCS1-4 supports 110/120/240 VAC Inputs. To use input power of 240 VAC, change the default 120 VAC 1.6-amp fuse to the supplied 500-milliamp fuse.