SMTP Email Alarm Configuration in Continuum 2.0


Instructions are needed to configure the new SMTP configuration

Product Line

Andover Continuum




Windows 7

Windows Server 2003

Windows Server 2008


Configuration for the new SMTP Configuration for email alarming in Continuum 2.0


The text version of the configuration and explanation is in the Cyberstation Help.

Here's a document that also has a couple added snapshots of the new dialogs

SMTP Configuration for Email Alarms 2.0

SMTP Configuration snapshots

Known issues:

In order for bacnet controllers to use the new smtp feature, the following hotfix from the following link is needed.

Some public smtp servers such as GMail SMTP and Yahoo SMTP do not currently work as they require SSL or certain ports. The way the connections to these servers is established causes a connection problem. Private smtp servers can be setup and used.