Issue
How does one know which joystick to order for a CM9760-KBD?
Product Line
Pelco Matrix
Environment
CM9760-KBD Keyboard
Cause
There are two different joysticks for CM9760-KBD,
Older model used 4 screws to mount and can be seen on bottom of CM9760-KBD case.
New model joystick mounts inside and no screws are seen on the back of CM9760-KBD case.
Calibration for new model joystick is different from old model joystick.
Resolution
CM9760-KBD NEW JOYSTICK PART NUMBER: ID02-4001-0002



CM9760-KBD OLD JOYSTICK PART NUMBER: WA01-1224-001K
For just the joystick boot: MF00-9850-016A