Schneider Universal Plug-In is registered in StruxureWare but we got an error message saying, that no plug in matches the program ID.

Issue

The Schneider Universal Plug-In 2.5.1 s registered in StruxureWare and the XIF file for the MTN880601 is imported into the StruxureWare database..

After adding the device and choosing Configure, the Plug-In is not launched.

Instead comes an error message saying, that no plug in matches the program ID.

Product Line

SmartStruxure Solution

Environment

StruxureWare
OpenLNS

Cause

XIF files that, during the installation, is not placed in the Import folder, may not be registered correctly in OpenLNS.

Resolution

In the StruxureWare Control Panel, under "LNS Plug-in Registration", you may have a selection "Import device templates in LNS."

Select this to import the XIF file (device template) into OpenLNS database.