DSSRV(2): Enable or Disable an IP Camera.

Issue

Activating or deactivating an IP camera on a Digital Sentry system.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DSSRV(2)
  • DigitalSentry
  • DS

Cause

  • Enable camera coming back from repair.
  • Disable camera that is temporaly not in use.

Resolution

  1. Open DS Admin, Start > Programs > Pelco > DS Admin
  2. Select the camera from the Cameras folder
  3. Select Edit IP Camera Settings
  4. Check or uncheck the Active checkbox.

 

Edit IP Camera Settings