Can I purchase additional mounting clips for the MNL-VxRVx or MNB-Vx controllers?

Issue

Can I purchase additional mounting clips for the MNL-VxRVx or MNB-Vx controllers?

Product Line

TAC I/A Series

Environment

MNL-VxRVx or MNB-Vx controllers

Cause

Each MNL-VxRVx and MNB-Vx controller includes one mounting clip that can be moved from the factory shipped location (bottom) to the side of the controller base.  The mounting clip is also known as the mounting foot or pivot bracket.

Resolution

Replacment or additional mounting clips can be purchased using part number DVAV-242.