How do I remove a camera from a monitor connected to a VCD5000 video-console display?

Issue

A camera is displayed in a matrix on a VCD5202 monitor. The user does not want to change to a different camera, but remove the camera completely from the grid.

Product Line

Pelco Video Management

Environment

VCD5202 video console display, all versions
VCD5000 video console display, all versions

Cause

Not applicable.

Resolution

First, select the square you wish to remove the camera from. Then, press 0 and the blue camera button shown in the figure below: