RH-Series Humidity Sensor Wiring Clarification

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

Confused by RF-Series sensor wiring instructions.

Do the controller's input return and the supplied power ground connect to the same termination on the sensor?

Product Line

Andover Continuum, Field Devices, SmartStruxure Solution

Environment

RH-Series sensor

Cause

Documentation

Resolution

*** If connecting to a voltage input on the controller then use the VOUT termination instead of the 4-20 mA