How do I Activate the Auxillery Monitor on a Genex Multiplexer

Issue

Setup the Aux monitor in the Genex program menu.

Product Line

Pelco Matrix

Environment

  • Genex
  • MX4016CD

Cause

Installation and  Service

Resolution

Enter the Programming menu using the front panal of the Genex. 

To program the main system parameters:

  1. Press the VIEW button for approximately three seconds until the System Setup menu appears. Type the password, if requested. The currently selected menu item blinks.
  2. Use the arrow buttons to move between items on the screen.
  3. Do one of the following when the menu item you desire is highlighted (blinking):
  • If a menu item has more than one option, press the +/- button to cycle through the options to select the one you want.
  • If a menu item has only one option, press the +/- button to select it.

Note that just parking on the option does not change it; you must also press the +/- button.

Use the arrow buttons to highlight ADVANCED SETUP, and press the +/- button. The Advanced System Setup menu appears.

  • Set the AUX MONITOR DISPLAY to the camera number or sequence desired.
  • Set RESPONDS TO field  to None
  • THIS WILL DISPLAY DESIRED CAMERA WITHOUT ANY INTERRUPTIONS.

Exit both menus and verify AUX monitor display.